Skip to main content
GreenGuy
Senior III
March 30, 2018
Question

Which selections in CubeMX do I use to be equivalent to LwIP_HTTP_Server_Netconn_RTOS application in the repository

  • March 30, 2018
  • 0 replies
  • 453 views
Posted on March 30, 2018 at 03:59

I can see in the Application project for STM32H743I_EVAL LwIP>LwIP_HTTP_Server_Netconn_RTOS that the application is using a custom fsdata.c file.  In the code elsewhere there is a define that directs the use of fsdata_custom.c as in httpd_opts.h:

/** Set this to 1 to include 'fsdata_custom.c' instead of 'fsdata.c' for the

 * file system (to prevent changing the file included in CVS) */

#if !defined HTTPD_USE_CUSTOM_FSDATA || defined __DOXYGEN__

#define HTTPD_USE_CUSTOM_FSDATA 0

#endif

I noticed in CubeMX that in the LWIP Configuration in the HTTPD tab, at the bottom of the page, there is a selection to enable HTTPD_USE_CUSTOM_FSDATA.  I assume that using that is akin to setting the define in https_opts.h.

My question is then what else do I need to set so I can build from CubeMX, port the appicaition specific code from the Application project, and compile to get the same result?

    This topic has been closed for replies.