Skip to main content
Visitor II
Jun 14, 2025 10:14 AM UTC
Solved

Which register can set the timeout for the FMC's NWAIT signal to prevent a crash?

Hi

Chip:stm32h723

Peripheral:FMC

Configuration:FMC_NORSRAM_DEVICE , FMC_NORSRAM_EXTENDED_DEVICE;

FMC_ACCESS_MODE_A

FMC_ASYNCRONOUS_WAIT_ENABLE

If the extended device(eg. FPGA) do not assert NWAIT,the program on stm32h723 will crash. I want to know which register can set the timeout for the NWAIT signal to prevent a crash?

 

Best regards,

Andy Zhou

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 17, 2025 3:54 PM UTC

Hello,

Unfortunately, there is no way to recover from that situation except to reset the CPU for example using the watchdog.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 17, 2025 3:54 PM UTC

Hello,

Unfortunately, there is no way to recover from that situation except to reset the CPU for example using the watchdog.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.