Skip to main content
T J
Senior III
Oct 21, 2018 12:36 AM UTC
Question

Which Processor have Floating Point in Hardware ?

Floating Point in Hardware, is it M3 and above ? L series ?

Which processors have Double Floating Point in Hardware ?

F7, H7 ?

    This topic has been closed for replies.

    4 replies

    T J
    T JAuthor
    Senior III
    Oct 21, 2018 12:49 AM UTC

    F3 F4 F7 are Single Precision FP in hardware

    F76x F77x and H7xx have the new DPFPU

    T J
    T JAuthor
    Senior III
    Oct 21, 2018 12:49 AM UTC

    F3 F4 F7 are Single Precision FP in hardware

    F76x F77x and H7xx have the new DPFPU

    L151 is based on M3 but has no FP in hardware

    T J
    T JAuthor
    Senior III
    Oct 21, 2018 1:48 AM UTC

    The STM32L443 has the hardware SPFP but less timers.

    The new STM32L4R series has 16+ timers. and DSI.

    Tilen MAJERLE
    ST Employee
    Oct 21, 2018 7:29 AM UTC

    Floating point is available in all devices based on Cortex-M4, M7 or M33 cores.

    Double floating point is available on some F7 and H7.