Which model in an ibis model file should I use?
Currently I am trying to use ibis model for simulation. I found ibis model file provided by STMicro and try to use them. But I could not figure out which model pointed by model selector I should use.
For example, there are 24 candidates of the model for PA0. But I don't know which one for my project.
Actual .ibs files is like below.
Thanks.
[Pin] signal_name model_name R_pin L_pin C_pin
...
6 PA0 io8p_wsudq_ls_ft_v33 61.160E-3 1.8629E-9 10.243E-15
...
[Model Selector] io8p_wsudq_ls_ft_v33
io8p00_wsudq_ls_ft_v33_pd_lv "SPEED00 1P8V, PD=40kOhm"
io8p00_wsudq_ls_ft_v33_pu_lv "SPEED00 1P8V, PU=40kOhm"
io8p00_wsudq_ls_ft_v33_lv "SPEED00 1P8V"
io8p01_wsudq_ls_ft_v33_pd_lv "SPEED01 1P8V, PD=40kOhm"
io8p01_wsudq_ls_ft_v33_pu_lv "SPEED01 1P8V, PU=40kOhm"
io8p01_wsudq_ls_ft_v33_lv "SPEED01 1P8V"
io8p10_wsudq_ls_ft_v33_pd_lv "SPEED10 1P8V, PD=40kOhm"
io8p10_wsudq_ls_ft_v33_pu_lv "SPEED10 1P8V, PU=40kOhm"
io8p10_wsudq_ls_ft_v33_lv "SPEED10 1P8V"
io8p11_wsudq_ls_ft_v33_pd_lv "SPEED11 1P8V, PD=40kOhm"
io8p11_wsudq_ls_ft_v33_pu_lv "SPEED11 1P8V, PU=40kOhm"
io8p11_wsudq_ls_ft_v33_lv "SPEED11 1P8V"
io8p00_wsudq_ls_ft_v33_pd "SPEED00, PD=40kOhm"
io8p00_wsudq_ls_ft_v33_pu "SPEED00, PU=40kOhm"
io8p00_wsudq_ls_ft_v33 "SPEED00"
io8p01_wsudq_ls_ft_v33_pd "SPEED01, PD=40kOhm"
io8p01_wsudq_ls_ft_v33_pu "SPEED01, PU=40kOhm"
io8p01_wsudq_ls_ft_v33 "SPEED01"
io8p10_wsudq_ls_ft_v33_pd "SPEED10, PD=40kOhm"
io8p10_wsudq_ls_ft_v33_pu "SPEED10, PU=40kOhm"
io8p10_wsudq_ls_ft_v33 "SPEED10"
io8p11_wsudq_ls_ft_v33_pd "SPEED11, PD=40kOhm"
io8p11_wsudq_ls_ft_v33_pu "SPEED11, PU=40kOhm"
io8p11_wsudq_ls_ft_v33 "SPEED11"