Skip to main content
Gunnar Bohlen
Associate III
Jun 23, 2017 2:05 PM UTC
Solved

Which memory can be used for periph to mem transfer?

Posted on June 23, 2017 at 16:05

Hello,

I use the CPU STM32F765.

I want to use DMA2 to transfer ADC-results into memory.

This works fine if I use DTCM-Memory for the destination  (128kbyte  from 0x20000000 to 0x2001ffff)

If I use SRAM1, DMA seems to work (I get transfer complete interrupt, ADC registers indicate that adc-values were read), but no data is in the programmed addresses.

Is it possible that ADC to DMA transfer only works when DTCM memory is used  for the destination?

Some time ago I maybe had a similar problem: I use Keil Middleware to implement a file system using an SD-card. It started to work after I told the middleware to use memory buffers at 0x20000000.

In the reference manual I read about DMA that it can address the complete memory range.

If it is required to specify DTCM memory for peripheral to memory transfers: where is this documented?

If SRAM1 should also work: What could be the reason why DMA works with DTCM, but not with SRAM1?

Thank you.

    This topic has been closed for replies.
    waclawek.jan
    waclawek.janBest answer
    Super User
    Jun 23, 2017 6:23 PM UTC
    Posted on June 23, 2017 at 20:23

    If SRAM1 is cached, the processor may see values from cache instead of values written newly by the DMA.

    You may want to read AN4839.

    JW

    3 replies

    waclawek.jan
    waclawek.janBest answer
    Super User
    Jun 23, 2017 6:23 PM UTC
    Posted on June 23, 2017 at 20:23

    If SRAM1 is cached, the processor may see values from cache instead of values written newly by the DMA.

    You may want to read AN4839.

    JW

    Gunnar Bohlen
    Associate III
    Jun 26, 2017 7:09 AM UTC
    Posted on June 26, 2017 at 09:09

    Thanks a lot.

    In the AN4839 I read:

    >Another case is when the DMA is writing to the SRAM1 and the CPU is going to read data

    >from the SRAM1. To ensure the data coherency between the cache and the SRAM1, the

    >software must perform a cache invalidate before reading the updated data from the SRAM1.

    This is exactly my case (ADC data transfered to SRAM1 via DMA2)

    Does this mean I cannot use the MPU to configure a small range of SRAM1 so that I can use it for DMA-Write and CPU-Read without invalidating the cache manually?

    GB

    waclawek.jan
    Super User
    Jun 26, 2017 10:41 AM UTC
    Posted on June 26, 2017 at 10:41

    Does this mean I cannot use the MPU to configure a small range of SRAM1 so that I can use it for DMA-Write and CPU-Read without invalidating the cache manually?

    The AN is not crystal clear. IMO you can. One of the obstacles may the limited number of regions (8 in those 'F7 I looked at) in the MPU, but that is usually enough for all practical applications with a bit of planning.

    JW