Skip to main content
MAmem.1
Associate III
Apr 8, 2022 2:29 PM UTC
Question

Which faster CAN 2.0 vs FDCAN Classic

I have two boards, one with STM32F303 with CAN 2.0 and a new board (same electronic, only MCU is different) with STM32G474. Software is identical too, except for the CAN/FDCAN. So I had to migrate the software from CAN 2.0 to FDCAN Classic in order to communicate with the other system boards.

In the treatment of the received frames, I noticed that the CAN 2.0 is faster in managing the communication than the FDCAN Classic.

Can anyone confirm that ? and if so why does it take so long to the FDCAN classic ?

As I send frames to both board, the STM32F303 program timing isn't affected, for the STM32G474 I measured a delay of some ms.

Clocks are as follow:

STM32F303 : CPU: 72 Mhz CAN baudrate: 500Kb/s

STM32G474 : CPU: 170 Mhz FDCAN classic baudrate: 500kb/s

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
Sep 23, 2026 2:25 PM UTC

Hello,

Nothing to do with the CAN protocol itself but more to your implementation in the software: need to check interrupt priorities, check if there is something disrupting the CAN reception routine by other loops/interrupts. In that case you need to use the interrupts.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.