Skip to main content
anton23
Associate II
October 22, 2016
Question

Where to get CoIDE

  • October 22, 2016
  • 2 replies
  • 806 views
Posted on October 22, 2016 at 20:25

It's strange but http://www.coocox.org/ do not work. Maybe there is a site from which this distribution can be downloaded? Besides http://www.coocox.org/. Thanks.

    This topic has been closed for replies.

    2 replies

    mckenney
    Associate
    October 25, 2016
    Posted on October 25, 2016 at 14:20

    The Coocox people seem to have disappeared about a year ago. I've visited a few times since then, but the site looked like a ghost town -- filled with spam and dead links. I'm not too surprised that someone finally pulled the plug.

    It's a bit odd that ST still mentions CoIDE, even on its newer product Web pages.

    I've been using OpenSTM32 (AC6).
    troy1818
    Associate III
    October 26, 2016
    Posted on October 26, 2016 at 11:21

    I think many vendors are getting their own solutions, making coIDE obsolete.

    Also, you do not really need it, the tool will just add to the compexity. For linux, just download the CMSIS for the MCU in question, get hold of the link file and the core headers, create a basic makefile and then -> make.

    See this link as an example (stm32f7):

    https://github.com/Staringlizard/memwa2

    As a debugger, just use gdb together with this:

    https://github.com/texane/stlink