Skip to main content
Associate III
March 28, 2024
Solved

Where is ETH_PHY_INTN

In the reference Manual of STMH730, on Table 543, page 2825, there's a Port "ETH_PHY_INTN" listed. Where ist that port? Or where can I configure the GPIO to use for it? I cannot find anything in the datasheet.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
April 16, 2024

Hello,

Just got the feedback regarding this topic and thank you for your patience.

The ETH_PHY_INTN pin is not available and it will be removed from the documentation. Meanwhile, this functionality could be managed by GPIO and EXTI.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

8 replies

Pavel A.
March 28, 2024

This is likely error in the RM. The Data sheet for H730 does not mention a pin function ETH_PHY_INTN.

If you want to receive interrupts from your PHY interrupt output, it can be connected to any suitable pin.

 

pkoevesdiAuthor
Associate III
March 29, 2024

@Pavel A. wrote:

This is likely error in the RM. The Data sheet for H730 does not mention a pin function ETH_PHY_INTN.

If you want to receive interrupts from your PHY interrupt output, it can be connected to any suitable pin.


Yes, but the RM says "Bit 3 PHYIS: PHY Interrupt
This bit is set when rising edge is detected on the ETH_PHY_INTN input. This bit is cleared when this register is read."

So, to use this function, I'd have to tell, where I have my INT input connected. So, either there's a dedicated pin function for it, which we cannot find in the datasheet, or I'd expect some register to tell, which GPIO I use for it.

 

Thank You for looking at it. For the first I assume, I can take any GPIO. Please tell here, if there's a special pin / function needed.

mƎALLEm
ST Technical Moderator
March 28, 2024

Hello,

I'm checking that internally. It could be a typo or a miss.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
pkoevesdiAuthor
Associate III
April 5, 2024

Any news on this?

mƎALLEm
ST Technical Moderator
April 5, 2024

I will keep you informed as soon as I have a feedback.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Pavel A.
March 29, 2024

The ETH IP supports multiple products. Some of them may have a dedicated PHY interrupt input, then it goes into that register bit.  Let's wait for SofLit to check.