Skip to main content
DBust.1
Visitor II
May 29, 2020
Question

Where do I find a working example of configuring and compiling the Opus codec library on a Linux machine for an STM32F407 target?

  • May 29, 2020
  • 1 reply
  • 668 views

Something along the lines of: ./configure CFLAGS="-O2 -mfpu=neon -mthumb -mcpu=cortex-m4" LDFLAGS="--specs=nosys.specs" --host=arm-none-eabi --disable-rtcd --enable-fixed-point

Still having issues with make errors, e.g.,

celt_pitch_xcorr_arm-gnu.S:547: Error: thumb conditional instruction should be in IT block

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
May 29, 2020

Determine if the assembler source file contains any conditional assembly code, and what command line defines those would need, or if you need to find a different source file for the Cortex-M devices.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..