Skip to main content
Jiannong Zhou
Associate III
February 18, 2023
Solved

Where can I find out or download MX25L6433F_STM32G071B_NUCLEO.stdlr?

Hi All,

I am using STM32G071RB-NUCLEO + X-NUCLEO-GFX01M2

Questions,

  1. Do we must use external loader and which loader file name we MUST use? is the loader file - MX25L6433F_STM32G071B_NUCLEO.stdlr correct?
  2. Where can I get this loader file.
  3. Why in sample project does not include this loader?

Best regards,

Jiannong

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
February 18, 2023

Sorry, this https://www.st.com/en/embedded-software/x-cube-display.html

Repository\Packs\STMicroelectronics\X-CUBE-DISPLAY\3.0.0\Utilities\PC_Software\ExternalLoader\MX25L6433F_GFX01M1_STM32G0.stldr

Repository\Packs\STMicroelectronics\X-CUBE-DISPLAY\3.0.0\Utilities\PC_Software\ExternalLoader\MX25L6433F_GFX01M2_STM32G0.stldr

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

5 replies

Tesla DeLorean
Guru
February 18, 2023

Try the X-CUBE-GFX package​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
February 18, 2023

Sorry, this https://www.st.com/en/embedded-software/x-cube-display.html

Repository\Packs\STMicroelectronics\X-CUBE-DISPLAY\3.0.0\Utilities\PC_Software\ExternalLoader\MX25L6433F_GFX01M1_STM32G0.stldr

Repository\Packs\STMicroelectronics\X-CUBE-DISPLAY\3.0.0\Utilities\PC_Software\ExternalLoader\MX25L6433F_GFX01M2_STM32G0.stldr

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AjcEng
Associate
July 10, 2024

Hi @Tesla DeLorean ,
Is the source code out there somewhere for the mentioned above MX25L6433F external loader ?
I created as example program to read and write to the MX25L6433F memory, which works as expected, but it would be helpful to see the source of the external loader program itself. 
I am in the process of creating my own loader using STM32CubeIDE, and have found some examples out there, but am still running into issues when it comes to the external loader part of this. It seems as if I am not initializing properly. 
For example, if I used the above mentioned loader, and the STM32CubeProgrammer, I can read and write. But when I switch to my program, it reads for a little and can write, but then it stops working. It's almost like there is something else blocking my write calls, and I am enabling the write before hand. 

Jiannong Zhou
Associate III
February 19, 2023

Hi Tesla,

Thank you very much!

After I used MX25L6433F_GFX01M1_STM32G0.stldr as external loader for Nucleo-G071BR + X-Nucleo-GFX01M2. STM32CubePogrammer works, it can downloaded the code into board. STM32CubeIde also can download the code into the board.

Jiannong