Skip to main content
Issinski.Anton
Associate III
August 14, 2018
Question

When using DMA to read from SPI - Data corrupted on STM32H743VI

  • August 14, 2018
  • 2 replies
  • 708 views

I trying to use STM32H743VI DMA1 to read from SPI2 MISO RXDR in master mode. 

Allocated memory in the D2 domain at address 0x3000000C for the DMA1 to copy SPI2 RXDR register to, but the resulting data is corrupted. I did not enable any D-cache at leaset manually myself, is it enabled by Atolic runtime or HAL? How to simply turn it all off? Tried to call SCB_DisableDCache() but it causes HardFault right away. __DSB() does not improve data integrity either. Anything else I may be missing?

Similar code for UART worked fine. Not using Cube at all, just the registers directly.

Thanks!

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    August 14, 2018

    Ok, you'd want to be a tad more selective.

    I think you'd need to use SCB_CleanDCache() before SCB_DisableDCache() otherwise you're likely to destroy stack content, and thus program execution context.

    ST's examples use an address scoped cache coherency method for DMA reads

    {
     /*
     the SCB_InvalidateDCache_by_Addr() requires a 32-Byte aligned address,
     adjust the address and the D-Cache size to invalidate accordingly.
     */
     uint32_t alignedAddr = (uint32_t)buff & ~0x1F;
     SCB_InvalidateDCache_by_Addr((uint32_t*)alignedAddr, size + ((uint32_t)buff - alignedAddr));
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Issinski.Anton
    Associate III
    August 15, 2018

    Thank you Clive.  SCB_CleanDCache() also causes HardFault. I call them the very first line in main(). I am leaning more towards disabling the cache for the affecting region so I don't have to invalidate it each time I receive a new byte.