Skip to main content
Associate III
Jul 17, 2025 1:14 PM UTC
Question

When transition from RDP level 1 to RDP level 0, how to avoid a POR ?

Hello,

MCU: STM32L071

During a transition from RDP level 1 to RDP level 0 the MCU stays stalled.

Only a power supply off then on permits to have it running.

Do you have any suggestion?

Best regards

Mich

This topic has been closed for replies.

2 replies

ST Technical Moderator
Jul 17, 2025 1:41 PM UTC

Hello @mich35 

As described in the reference manual RM0377: 

Note: If the read protection is set while the debugger has been active (through SWD) after last POR (power-on reset), apply a POR (power-on reset) or wakeup from Standby mode instead of a system reset (the option bytes loading is not sufficient).

Try reload the option bytes after programming, for that you can refer to the "3.8.3 Reloading Option bytes by software"section in the reference manual RM0377.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
mich35Author
Associate III
Jul 17, 2025 3:11 PM UTC

Hello Imen,

I was not with the debugger.

I try to put the system in Standby mode but it does not work, the MCU is stalled. (it works fine from level 0 to level 1)

I follow "STM32 Security tips - 3 RDP without POR" video (level 0 to level 1) but there is nothing for level 1 to level 0.

Best regards

Michel