When ST HAL will be fully compatible with RTOS???
I had some trouble with SPI before and now I have same kind of trouble with I2C. I use FreeRTOS and HAL drivers, all generated by CubeMX. Function and my fix in bold:
static HAL_StatusTypeDef I2C_WaitOnRXNEFlagUntilTimeout(I2C_HandleTypeDef *hi2c, uint32_t Timeout, uint32_t Tickstart)
{
while(__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_RXNE) == RESET)
{
/* Check if a NACK is detected */
if(I2C_IsAcknowledgeFailed(hi2c, Timeout, Tickstart) != HAL_OK)
{
return HAL_ERROR;
}
/* Check if a STOPF is detected */
if(__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_STOPF) == SET)
{
// But without any received byte. ST HAL doesn't expect // context switching. So, if context will be switched after // entering into while() cycle but before STOPF check happen // when we receiving last byte, STOPF will be set after this // byte received. When context will be switched back, this // code will found STOPF and return an error. For prevent that, // after STOPF condition detected we should check RXNE bit, // and if we have byte - this is not an error. if(__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_RXNE) == RESET) {/* Clear STOP Flag */
__HAL_I2C_CLEAR_FLAG(hi2c, I2C_FLAG_STOPF);
/* Clear Configuration Register 2 */
I2C_RESET_CR2(hi2c);
hi2c->ErrorCode = HAL_I2C_ERROR_NONE;
hi2c->State= HAL_I2C_STATE_READY;
hi2c->Mode = HAL_I2C_MODE_NONE;
/* Process Unlocked */
__HAL_UNLOCK(hi2c);
return HAL_ERROR;
}}
So, I have same kind of issue second time! Your developers should pay more attention and start thinking 'in multi-threading'.
Thanks