Skip to main content
aulus.18
Associate
July 1, 2019
Question

when SRAM & TFT connected to FSMC, One of them doesn't work properly

  • July 1, 2019
  • 2 replies
  • 1064 views

Hello,

My board includes SRAM, TFT (5.0 inch with ssd1963), NOR, NAND circuits.

When TFT is not connected, SRAM passes all tests (all memory read/write).

(I didn't test NOR or NAND)

if TFT is connected, Sram test fails any address. (Or TFT doesn't work properly in sram test)

(The project includes stemwin)

While writing/reading to sram, I think TFT too or the exact opposite.

Data , addresses, Read,write etc pins are common but all chip selects is following.

PG9 <-> FSMC_NE2 // NOR-CS

PG10 <-> FSMC_NE3 // SRAM-CS

PD7 <-> FSMC_NCE2 // NAND-CS

PG12 <-> FSMC_NE4 // TFT-CS

I wanted to ask that don't look hardware. in fact, I checked hardware before. All connections were OK. Isn't this state related CS? (by the way, there is not hardfault state)

how can such a situation occur?

Thanks.

This topic has been closed for replies.

2 replies

aulus.18
aulus.18Author
Associate
July 1, 2019

i read the following article from a chinese source, ( between comments)

/*

 * PG9 is connected to the CE side of NORFLASH in order to prevent the NORFLASH signal from affecting the SRAM.

 * Here let CE = 1 first, that is, PG9 = 1, otherwise the SRAM will not test successfully.

 * Or when the hardware is designed, the NORFLASH CE pin is pulled down.

 */

Why Sram and nor affect each other?

For PG9 is AF, if I don't write/read to NOR ( to only SRAM address), PG9 ( FSMC_NE2 - NOR_CS) can be enable?

PG9 <-> FSMC_NE2 // NOR-CS

PG10 <-> FSMC_NE3 // SRAM-CS

Tesla DeLorean
Guru
July 1, 2019

None of us here know what STM32 chip, board and source you are using.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
aulus.18
aulus.18Author
Associate
July 1, 2019

You're right, Sorry,

Stm32F407ZET6, The connections is following,

TFT and SRAM are working alone but together, tft freezes (mcu is working) and sram test is getting faulty

TFT Connections:
PD14 <-> FSMC_D0 // DATA-0
PD15 <-> FSMC_D1 // DATA-1
PD0 <-> FSMC_D2 // DATA-2 
PD1 <-> FSMC_D3 // DATA-3
PE7 <-> FSMC_D4 // DATA-4
PE8 <-> FSMC_D5 // DATA-5
PE9 <-> FSMC_D6 // DATA-6
PE10 <-> FSMC_D7 // DATA-7
PE11 <-> FSMC_D8 // DATA-8
PE12 <-> FSMC_D9 // DATA-9
PE13 <-> FSMC_D10 // DATA-10
PE14 <-> FSMC_D11 // DATA-11
PE15 <-> FSMC_D12 // DATA-12
PD8 <-> FSMC_D13 // DATA-13
PD9 <-> FSMC_D14 // DATA-14
PD10 <-> FSMC_D15 // DATA-15
// tft control pins
PF0 <-> FSMC_A0 // LCD-RS
PG12 <-> FSMC_NE4 // LCD-CS 
PD4 <-> FSMC_NOE // LCD-OE 
PD5 <-> FSMC_NWE // LCD-WE 
 
K91G08U0B:
PD11 <-> FSMC_A16				// NAND-CLE
PD12 <-> FSMC_A17				// NAND-ALE 
PD6 <-> FSMC_NWAI 			 // NAND-RB 
PD4 <-> FSMC_NOE				// NAND-OE 
PD7 <-> FSMC_NCE2			 // NAND-CS 
PD5 <-> FSMC_NWE				// NAND-WE 
 
SST39VF1601 :
PF0 <-> FSMC_A0				// NOR-ADDRESS-0
PF1 <-> FSMC_A1				// NOR-ADDRESS-1
PF2 <-> FSMC_A2				// NOR-ADDRESS-2
PF3 <-> FSMC_A3				// NOR-ADDRESS-3
PF4 <-> FSMC_A4				// NOR-ADDRESS-4
PF5 <-> FSMC_A5				// NOR-ADDRESS-5
PF12 <-> FSMC_A6				// NOR-ADDRESS-6
PF13 <-> FSMC_A7				// NOR-ADDRESS-7
PF14 <-> FSMC_A8				// NOR-ADDRESS-8
PF15 <-> FSMC_A9				// NOR-ADDRESS-9
PG0 <-> FSMC_A10				// NOR-ADDRESS-10
PG1 <-> FSMC_A11				// NOR-ADDRESS-11
PG2 <-> FSMC_A12				// NOR-ADDRESS-12
PG3 <-> FSMC_A13				// NOR-ADDRESS-13
PG4 <-> FSMC_A14				// NOR-ADDRESS-14
PG5 <-> FSMC_A15				// NOR-ADDRESS-15
PD11 <-> FSMC_A16				// NOR-ADDRESS-16
PD12 <-> FSMC_A17				// NOR-ADDRESS-17
PD13 <-> FSMC_A18				// NOR-ADDRESS-18
PE3 <-> FSMC_A19				// NOR-ADDRESS-19
PE4 <-> FSMC_A20				// NOR-ADDRESS-20
PE5 <-> FSMC_A21				// NOR-ADDRESS-21
PE6 <-> FSMC_A22				// NOR-ADDRESS-22
 
PG9 <-> FSMC_NE2				// NOR-CS
 
IS61WV51216EDALL:
PG10 <-> FSMC_NE3				// SRAM-CS 
PE0 <-> FSMC_NBL0			 // SRAM-LB 
PE1 <-> FSMC_NBL1			 // SRAM-UB