Skip to main content
Misha K
Associate II
May 15, 2018 11:48 AM UTC
Solved

When reading USART, DMA instantaneously completes

Posted on May 15, 2018 at 13:48

Please see code below.

I'm trying to read from USART using DMA. 

Please see the last line DMA1_Channel3->CCR |= DMA_CCR_EN;

When I step over that line, 

CNDTR instantaneously resets to zero like it has finished reading, also destination buffer is populated by multiple instances of the same char that was in USART1->RDR.

It looks like DMA believes that the same char is constantly arriving into RDR and available for transfer.

I don't expect any actual USART transmission at that time.

What am I doing wrong please?

void ScheduleUsartDmaRead(){

USART1->CR1 &= ~USART_CR1_TE;

USART1->CR1 |= USART_CR1_RE;

USART1->CR1 |= USART_CR1_UE; // enable usart

DMA1_Channel3->CCR &= ~DMA_CCR_EN; // disable DMA to set registers

DMA1_Channel3->CCR &= ~DMA_CCR_DIR; // peripheral to memory

DMA1->IFCR = DMA_FLAG_GL3; // clear flags

DMA1_Channel3->CNDTR = usartBufferSize; // set buffer size

DMA1_Channel3->CPAR = (uint32_t)(&(USART1->RDR)); // USART register address

DMA1_Channel3->CMAR = (uint32_t)(usartInBuffer); // memory address

DMA1_Channel3->CCR |= DMA_CCR_EN; // start DMA

}
    This topic has been closed for replies.
    Misha K
    Misha KBest answer
    Associate II
    May 15, 2018 1:20 PM UTC
    Posted on May 15, 2018 at 15:20

    Answering my own question.

    I used same DMA channel for USART and SPI.

    I was thinking that when processing USART it was enough to disable SPI and point DMA->

    CPAR to USART register.

    Surprisingly just disabling SPI is not enough, I also had to clear its RXDMAEN and TXDMAEN flags.

    2 replies

    Tesla DeLorean
    Guru
    May 15, 2018 12:47 PM UTC
    Posted on May 15, 2018 at 14:47

    What STM32 part is being used here?

    Not looking to dig into others register level code, try using the HAL/LL until you have it working

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Misha K
    Misha KAuthorBest answer
    Associate II
    May 15, 2018 1:20 PM UTC
    Posted on May 15, 2018 at 15:20

    Answering my own question.

    I used same DMA channel for USART and SPI.

    I was thinking that when processing USART it was enough to disable SPI and point DMA->

    CPAR to USART register.

    Surprisingly just disabling SPI is not enough, I also had to clear its RXDMAEN and TXDMAEN flags.