Skip to main content
jean_prieur
Associate III
Sep 11, 2013 3:32 PM UTC
Question

When I touch the SCL pin with my finger the SPI works

Posted on September 11, 2013 at 17:32

Hello,

I programmed a LCD screen with SPI on a prototype and everything was working fine.

But I mounted

 the screen on the final PCB and now I have a 

problem: the screen didn't understand the datas I send to it. The screen 

remains white. Datas are correctly send, I know it because I compare signals 

with my working prototype.

When I touch with my finger the clock pin, the screen is able to 

understand datas and works fine.

Do you ever had this problem ? I am sure of the screen connexions and 

I tested it with different SPI speeds and configurations...

Thanks !
    This topic has been closed for replies.

    12 replies

    Tesla DeLorean
    Guru
    Sep 11, 2013 4:05 PM UTC
    Posted on September 11, 2013 at 18:05

    Ineffective ground paths, or other supply issues?

    The information supplied doesn't really convey any engineering design information.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jean_prieur
    Associate III
    Sep 11, 2013 4:28 PM UTC
    Posted on September 11, 2013 at 18:28

    Hello Clive,

    Sorry for the missing engineering information, i was just to explain my problem easily.

    I'm not sure it is a ground or supply or signal problem, because I try to link my screen with other wire solutions and the problem is still here...

    On the PCB, coppers from the uC (stm32f427vit6) and the screen (DOGM128-6) width is 0,2mm and the length is 20cm... Maybe it's too thin but when I add floating wires there is no change. 

    jj2
    Associate
    Sep 11, 2013 4:29 PM UTC
    Posted on September 11, 2013 at 18:29

    Use of your finger as test probe or temperature sense - may prove sub-optimal.  ESD anyone?

    Might it be that the added body capacitance extends or alters a critical signal - which is, ''at the edge'' of timing spec?  Or - may indicate that the added stress causes a faulty connection/contact to ''restore.''

    emalund
    Associate III
    Sep 11, 2013 5:54 PM UTC
    Posted on September 11, 2013 at 19:54

    The f4 is pretty fast, many LCDs are a bit slow.

    check the specs for the LCD and verify you adhere to the timing requirements.

    Erik
    jj2
    Associate
    Sep 11, 2013 6:18 PM UTC
    Posted on September 11, 2013 at 20:18

    @ Erik,

    At first glance - my response was almost, ''word for word'' yours.

    But.... his is SPI input Lcd - and any/all timing should be managed by that intervening device - avoiding the ''usual'' lcd s...l...o...w... accommodation.

    @Poster,

    Just checked display & 7565 data.  Note 2 critical issues:

    a) 7565 accepts up to 20MHz SPI clock - but I'd stay below 10MHz during test/verify.

    b) depending upon your powering of this display - you need either 9 1uF caps (3V3 power) or 5 1uF caps (10V +) which tie to critical charge pump pins (mostly) on the display.

    I'd place small wager that your MCU SPI clock is set too close to max of the Lcd controller - dialing down would be my first attempt...

    jean_prieur
    Associate III
    Sep 12, 2013 9:23 AM UTC
    Posted on September 12, 2013 at 11:23

    1) Of course my screen have the 1uF capacitors connected because I'm in 3V3. I put standard 0805 CMS ceramic capacitors, I hope this is not the problem.

    2) I try to communicate with lower speeds but no changes. What is the right way to lower the speed ? Is it to change the SPI_BaudRatePrescaler or to set the GPIO_Speed pins to a lower speed ?

    This is strange because at the maximal speed (SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2 and GPIO_Speed = 100MHz) the screen works when I put my finger on the pins...

    3) It's not possible in my design to place the microcontroller near my screen. I have to do with that.

    jj2
    Associate
    Sep 12, 2013 1:54 PM UTC
    Posted on September 12, 2013 at 15:54

    Jean: ''Of course my screen have the 1uF capacitors connected...''

     

    Not the most appropriate nor diplomatic response - none here could have so known!

    Review of the SPI section w/in MCU manual should reveal how you can alter SPI clock speed.

    I made time/effort to review 7565 spec - and noted a caution as to, ''reflections'' upon the SPI clock line.  Usually a terminating resistor helps in this regard.  Suggest you ''start'' at/around 100 ohms - ranging up to 10K.  This R should be located close to the Lcd controller (and possibly was included by display vendor - resistance measurement between clock line & ground will reveal if this R exists)

    And - of course - you are welcome...

    jean_prieur
    Associate III
    Sep 12, 2013 6:56 PM UTC
    Posted on September 12, 2013 at 20:56

    Thanks a lot for these advices jj.sprague ! Sorry for the ''of course'' it was really not appropriate, not my real intention...

    I will try it tomorow and keep you informed.

    David Littell
    Senior II
    Sep 12, 2013 8:30 PM UTC
    Posted on September 12, 2013 at 22:30

    Sounds like your clock line could benefit from a close examination with a good scope with a FET probe.  Beg/borrow/steal/rent/buy and you might be shocked at what you see.

    jj2
    Associate
    Sep 12, 2013 11:12 PM UTC
    Posted on September 13, 2013 at 01:12

    Dave: ''Sounds like your clock line could benefit from a close examination with a good scope...''   (Suspect you may be the ''source'' - on sister fora...)

    Surely you don't mean to impugn the value/capability of a ''finger'' as test probe...

    Mating an M4/F4 with such non-standard methods... little to be said...