Visitor II
Feb 8, 2017 7:27 PM UTC
Question
When enable USBHS internal IP DMA, STM32F746 discovery board fail to enumerate.
- 4 replies
- 2162 views
Posted on February 08, 2017 at 20:27
I use STM32CubeMX to generate STM32F46 discovery board project, just enable 'USBHS internal IP DMA', Choose CDC class, show as the attached picture 01, when I compile and run the firmware, connect the USB HS port, I use the USBView.exe from win10 to check the USB information, it shows 'FailedEnumeration', show as the pitcture02. If I disable
'USBHS internal IP DMA', then everything will be fine. Can anybody tell me how use the USBHS internal IP DMA?Is any other setting I should do? Thanks!