Solved
When downloading FW on the stm32L476ZGT EVAL,
When downloading FW on the stm32L476ZGT EVAL by using CubeIDE1.10.1ver,
I faced with Error: Failed to download Segment[0], Error: Failed to download the File...,
How can I solve these problems? Even I didn't write any code in there.
Following is my Console window...
If you guys have any good ideas, please save me...
I uninstalled CubeIDE 1.07ver and installed CubeIDE 1.10ver but it wasn't working.
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0
-------------------------------------------------------------------
Log output file: C:\Users\Owner\AppData\Local\Temp\STM32CubeProgrammer_a11136.log
ST-LINK SN : 56FF6C066683565232541987
ST-LINK FW : V2J40S7
Board : --
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x415
Revision ID : Rev 2
Error: Database: There's no active configuration for this device. All the 5 configurations are disabled!
Error: Database: There's no active configuration for this device. All the 5 configurations are disabled!
Device name : STM32L4x1/STM32L475xx/STM32L476xx/STM32L486xx
Flash size : 63 KBytes (default)
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
Mass erase ...
Mass erase successfully achieved
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0
-------------------------------------------------------------------
Log output file: C:\Users\Owner\AppData\Local\Temp\STM32CubeProgrammer_a11136.log
ST-LINK SN : 56FF6C066683565232541987
ST-LINK FW : V2J40S7
Board : --
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x415
Revision ID : Rev 2
Error: Database: There's no active configuration for this device. All the 5 configurations are disabled!
Error: Database: There's no active configuration for this device. All the 5 configurations are disabled!
Device name : STM32L4x1/STM32L475xx/STM32L476xx/STM32L486xx
Flash size : 63 KBytes (default)
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a11136.srec
File : ST-LINK_GDB_server_a11136.srec
Size : 11.59 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing external memory sectors [0 5]
File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
Shutting down...
Exit.