Skip to main content
JNoon.1
Associate III
June 1, 2023
Solved

When debugging custom hardware using a STM32L431KC, the debugger gets stuck in the reset_handler.

When debugging custom hardware with the STM32L431KC, the debugger gets stuck in the reset handler:

Reset_Handler:
 ldr sp, =_estack /* Set stack pointer */

And in the console it says:

Open On-Chip Debugger 0.12.0-rc1+dev-00061-g5e9b46d77 (2022-10-20-14:50) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J10M3 (API v3) VID:PID 0483:374E
Info : Target voltage: 3.274617
Info : clock speed 8000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x2ba01477
Info : [STM32L431KCUx.cpu] Cortex-M4 r0p1 processor detected
Info : [STM32L431KCUx.cpu] target has 6 breakpoints, 4 watchpoints
Info : starting gdb server for STM32L431KCUx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : [STM32L431KCUx.cpu] external reset detected
Info : accepting 'gdb' connection on tcp/3333
[STM32L431KCUx.cpu] halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x080020a4 msp: 0x20010000
Info : device idcode = 0x10016435 (STM32L43/L44xx - Rev Z : 0x1001)
Info : RDP level 0 (0xAA)
Info : flash size = 256 KiB
Info : flash mode : single-bank
Info : accepting 'gdb' connection on tcp/3333
Warn : GDB connection 2 on target STM32L431KCUx.cpu not halted

Any help/reasons to why it does this?

It will suddenly work and then not work for hours....

Any help is appreciated.

Thanks

This topic has been closed for replies.
JNoon.1
JNoon.1Best answer
Associate III
September 11, 2023

Forgot to post an answer to this....

For some unknown reason when the live expressions tab is open the debugging session will not start but if I change it to the breakpoint view for example and try to debug again... it works! 

Weird solution but works for me!

3 replies

waclawek.jan
Super User
June 2, 2023

Wild guess: spurious bootloader entry?

JW

JNoon.1
JNoon.1AuthorBest answer
Associate III
September 11, 2023

Forgot to post an answer to this....

For some unknown reason when the live expressions tab is open the debugging session will not start but if I change it to the breakpoint view for example and try to debug again... it works! 

Weird solution but works for me!

Garnett.Robert
Senior III
September 21, 2023

Hi,

 

Unhandled interrupt?

Regards

Rob