Skip to main content
FatihTaşt.
Associate
July 29, 2024
Question

When data is deleted in Flash, this directly affects my GPIO pins.

I am working with STM32G030K6T6 MCU. In some cases I write and erase to flash memory. While writing there is no problem, while erasing some of my GPIOs go from HIGH to LOW momentarily. I see LED blinking momentarily. Erase function works fine but my general purpose peripheral is affected. My write and erase functions are almost the same as STM32Cube->Repository example. No change is observed in MCU power supply. Can you help me? Thanks.

This topic has been closed for replies.

4 replies

Andrew Neil
Super User
July 29, 2024

@FatihTaşt. wrote:

My write and erase functions are almost the same as STM32Cube->Repository example. 


"almost" ?  :thinking_face:

So what, exactly, is different?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
July 29, 2024

Probably going to need more detail here. Which pins are affected and at which point exactly within the code.

"If you feel a post has answered your question, please click ""Accept as Solution""."
FatihTaşt.
Associate
July 29, 2024

This happens when I call the HAL_FLASHEx_Erase() function and I get the message "Target not responding, retrying......" from St-Link for a short while. The LED I control on port B resets briefly.Also the ST-link SWD pins are probably affected by this situation.

FLASH_EraseInitTypeDef erase_init;
uint32_t page_error = 0;

/* Set page erase initialization structure */
erase_init.TypeErase = FLASH_TYPEERASE_PAGES;
erase_init.PageAddress = page_address;
erase_init.NbPages = page_count;

HAL_FLASH_Unlock();
/* Flash erase initialization */
if (HAL_FLASHEx_Erase(&erase_init, &page_error) != HAL_OK)
{
/* Error condition handling */
// Error_Handler();
}

HAL_FLASH_Lock();

 The error received is indicated;

Ekran görüntüsü 2024-07-30 165533.png

Andrew Neil
Super User
July 30, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.