Skip to main content
RBamf.1
Associate III
February 12, 2020
Question

What to use for HAL_SAI_Receive Size parameter?

  • February 12, 2020
  • 1 reply
  • 801 views

Hi, I'm trying to work with the SAI HAL interface, i have set the black frame to 64 bits wide and the block slot size to 32B.

When using the HAL_SAI_Receive() function, what does the length parameter represent?

For my solution i am sending 2 32bit slots in 1 64 bit frame, therefore is the length parameter set to 64 bits?

Here's the SAI function in question:

/**
 * @brief Receive an amount of data in blocking mode.
 * @param hsai pointer to a SAI_HandleTypeDef structure that contains
 * the configuration information for SAI module.
 * @param pData Pointer to data buffer
 * @param Size Amount of data to be received
 * @param Timeout Timeout duration
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_SAI_Receive(SAI_HandleTypeDef *hsai, uint8_t *pData, uint16_t Size, uint32_t Timeout)

It is found in stm32l4xx_hal_sai.c line 1133.

My setup is an Nucleo-64 STM32L452RE.

Many Thanks!

Richard

This topic has been closed for replies.

1 reply

RBamf.1
RBamf.1Author
Associate III
February 13, 2020

Anyone?