Question
What's wrong with my SPI setup?!
Hi,
I'm really struggling with the simplest possible way to use SPI with STM32F745 as a master and a MPU6000 as a slave - no interrupts, no DMA, just plain while loops and busy waiting.
Problem: I can't get it to work, the SCK signal is plain dead!
Code:
Initialization:
==========
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN;
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN;
waitCycles();
// Set Alternate Function for all SPI GPIO pins
// SS -> PA4
// CLK -> PA5
// MISO -> PA6
// MOSI -> PA7
constexpr uint32_t kAlternateFunction = 0b10;
constexpr uint32_t kGeneralOutput = 0b01;
GPIOA->MODER |=
(kAlternateFunction << GPIO_MODER_MODER4_Pos | kAlternateFunction << GPIO_MODER_MODER5_Pos |
kAlternateFunction << GPIO_MODER_MODER6_Pos | kAlternateFunction << GPIO_MODER_MODER7_Pos);
GPIOA->OTYPER = 0x0000'0000;
constexpr uint32_t kSpeed = 0b11; // Very high speed
GPIOA->OSPEEDR |= (kSpeed << GPIO_OSPEEDER_OSPEEDR4_Pos | kSpeed << GPIO_OSPEEDER_OSPEEDR5_Pos |
kSpeed << GPIO_OSPEEDER_OSPEEDR6_Pos | kSpeed << GPIO_OSPEEDER_OSPEEDR7_Pos);
constexpr uint32_t kPullUp = 0b01;
GPIOA->PUPDR |= (kPullUp << GPIO_PUPDR_PUPDR4_Pos | kPullUp << GPIO_PUPDR_PUPDR5_Pos |
kPullUp << GPIO_PUPDR_PUPDR6_Pos | kPullUp << GPIO_PUPDR_PUPDR7_Pos);
constexpr uint32_t kAlternateFncSpi = 5U;
GPIOA->AFR[0U] |=
(kAlternateFncSpi << GPIO_AFRL_AFRL4_Pos | kAlternateFncSpi << GPIO_AFRL_AFRL5_Pos |
kAlternateFncSpi << GPIO_AFRL_AFRL6_Pos | kAlternateFncSpi << GPIO_AFRL_AFRL7_Pos);
// 2) Configure SPI_CR1 register
SPI1->CR1 |= ((7U << SPI_CR1_BR_Pos) | // Prescaler
SPI_CR1_MSTR | // Configure as master
SPI_CR1_CPOL | // Polarity = 1
SPI_CR1_SSM |
SPI_CR1_CPHA); // Phase = 1
// 3) Configure SPI_CR2 register
constexpr uint32_t kDataSizeOption = 0b0111; // 8-bit data size
SPI1->CR2 |=
((kDataSizeOption << SPI_CR2_DS_Pos) |
SPI_CR2_FRXTH
);
// Enable SPI
SPI1->CR1 |= SPI_CR1_SPE;Transfer:
=======
uint8_t transfer(const uint8_t data)
{
while ((SPI1->SR & SPI_SR_BSY) != 0U){}
// Write data
*(volatile uint8_t *)(&SPI1->DR) = data;
// Wait for transmission
// while ((SPI1->SR & SPI_SR_TXE) == 0U){}
// Wait for reception
// while ((SPI1->SR & SPI_SR_RXNE) == 0U){}
// Wait until line is not busy
while ((SPI1->SR & SPI_SR_BSY) != 0U){}
// Return read data
const uint8_t data_received = *(volatile uint8_t* )(&SPI1->DR);
return data_received;
}What am I missing?
Also, can someone please explain how to use the TXE and RXNE flags? I have read the reference manual a lot of times but I really don't understand what's written.
Thanks!