Question
What's the max voltage tolerance when STM32 is not powered?
I'm confused with the max voltage tolerance of STM32's GPIO.
- In the datasheet, it states the max voltage of Vin is 4V for TT_xx pins. But in AN4899, it states they are Vdd + 0.3V. You see, the former has no relation with Vdd, it implies they will tolerant 4V even Vdd is 0V. But the later tells me, when Vdd is 0V, Vin can't go beyond 0.3V.
- In the datasheet, it states the max voltage of Vin is 5.5V for FT_c pins and has no relation with Vdd. But in AN4899, it states when Vdd = 0V, the pins can only tolerant 3.6V.
Any help? Thanks.