Question
What's the bXCAN RXD recessive signal on STM32L476?
I'm reading RM0351 for STM32L476, "To be synchronized the hardware has to monitor a sequence of 11 consecutive recessive bits on the CAN RX signal." Is RX recessive bit a digital high or low signal? I couldn't find the info on the datasheet which only says "Refer to Section 6.3.14: I/O port characteristics for more details on the input/output alternate
function characteristics (CAN_TX and CAN_RX)."