What's the best protocol (USART mode?) for high-speed bidirectional comm between two STM32s?
I’m designing a motor control PCB with two STM32G432RBs (situated close to each other on the PCB) driving a boatload of H-Bridges, encoders, servos, and other I/O. I’m planning a dedicated (synchronous) USART connection between the two STM32G4s to keep them coordinated. Speed and bidirectional comm matter in this setting (power not as much). What is the maximum data rate (Mbps) that I can reasonably expect in this set up (I can only find one mention of a "max USART clock freq", of 21 MHz, in the datasheet),
[Or should I use SPI instead? I am confused by the phrase "SPI-like" in the sentence from the datasheet "The USART1, USART2 and USART3 also provide a Smartcard mode (ISO 7816 compliant) and an SPI-like communication capability."....]
Finally: USART can run in many different "modes"; what is the best ("native"?) USART comm mode to use in such a setting?