Skip to main content
KMak
Visitor II
November 26, 2018
Question

What‘s the actual GBW of OPAMP in STM32F303?

  • November 26, 2018
  • 1 reply
  • 1000 views

0690X000006CTW4QAO.bmp

(yellow line: non inverting input

blue line: output of OPAMP )

Hi,

I am using the NUCLEO-F303RE board and now I am testing the OPAMP3 , which is one of the peripherals in STM32F303.

I have set the PA1 as non inverting input, PB2 as inverting input. And I input differential signal (up to 400kHz) to OPAMP3. It seems that the voltage OPAMP output is too low.

According to​ official manual, the GBW of OPAMP is 8Mhz. But now this OPAMP has bad performance when input signal is 400kHz.

How do you think about it?

​

​

    This topic has been closed for replies.

    1 reply

    AvaTar
    Senior III
    November 26, 2018

    A 400kHz rectangular signal is not "400kHz" in terms of bandwidth.