Skip to main content
JBias
Associate III
Jan 17, 2025 6:36 PM UTC
Solved

What parameters to use for the external MX661G45... Flash on the STM32H7S78-DK

Datasheet for the Macronix flash is not available on-line. Can someone tell me about the correct parameters needed for the Macronix MX66UW1G flash?

The number of sectors (used 32), sector size (used 4096), page size (used 0x100), chip select high time (used 2), delay hold quarter cycle (enabled) and any other useful information to get the external memory loader to work?

I'm getting a failure to erase flash sector0

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 17, 2025 11:12 PM UTC

MX66 means it's a stacked-die, so 1Gb (128MB), 2x 512Mbit

Can you pull a SFDP? And get the parameters from there?

Instrument the loader, understand what exactly is failing

I suspect the parameters will look materially the same as the LM/UM models, with the benefit of have some concurrent READ/WRITE/ERASE on uninvolved die

https://github.com/STMicroelectronics/stm32-mx66uw1g45g

https://github.com/STMicroelectronics/stm32h7s78-dk-bsp/blob/58902b169f56a9aa064970f63567d93ab219bf21/stm32h7s78_discovery_xspi.c

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 17, 2025 11:12 PM UTC

MX66 means it's a stacked-die, so 1Gb (128MB), 2x 512Mbit

Can you pull a SFDP? And get the parameters from there?

Instrument the loader, understand what exactly is failing

I suspect the parameters will look materially the same as the LM/UM models, with the benefit of have some concurrent READ/WRITE/ERASE on uninvolved die

https://github.com/STMicroelectronics/stm32-mx66uw1g45g

https://github.com/STMicroelectronics/stm32h7s78-dk-bsp/blob/58902b169f56a9aa064970f63567d93ab219bf21/stm32h7s78_discovery_xspi.c

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Jan 17, 2025 11:24 PM UTC

Loader Source for .FLM the older step-brother of the .STLDR, the .pack is a ZIP file

https://github.com/STMicroelectronics/STM32CubeH7RS/blob/main/Utilities/PC_Software/Keil.STM32H7RSxx_DFP.1.0.0.zip

Keil.STM32H7RSxx_DFP.1.0.0.pack\CMSIS\Flash\STM32H7S78_DK_OSPI\OSPI - ZIP archive

This data sheet is likely to be sufficiently informative, the .C / .H in the BSP and PACK likely covering any gaps

https://www.macronix.com/Lists/Datasheet/Attachments/8742/MX66U1G45G,%201.8V,%201Gb,%20v1.4.pdf

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..