What is the use of PDR ON ?
hello .
1.We have done a Stm32F429 board , and we can set PDR ON to GND OR VCC (we set to gnd)
how ever in the STM32 PDF : AN4488 Application note STM32F4xxxx MCU hardware
it says in IN ....3.2.1 PDR_ON
PDR_ON = 0 is mostly intended for VDD supply between 1.7 V and 1.9V (i.e. 1.8V +/- 5% supply). Supply ranges which never go below 1.8V minimum should be better managed with internal circuitry (no additional component thanks to fully embedded reset controller). • To ensure safe power down, the external voltage supervisor (or equivalent) is required to drive PDR_ON=1 during power off sequence
1.1 we done PDR ON CONNECT to GND we use 3.3V -3.0 V to the mcu did we set pdr_on correct ?
when should i use pdr_on to vcc and when to gnd please explain in more practical example .
thanks
yaniv