Skip to main content
Yang Yang
Associate III
Apr 8, 2025 6:36 AM UTC
Solved

What is the temperature sensor calibration value if VREF is not 3.0V as datasheet refered

Hello, ST experts

 

The temperature sensor in STM32U595 is used for a mesurement. As datasheet said TS_CAL1 can be read at address 0x0BFA0710~0x0BFA0711. But this value is for 3.0V VREF, how is the situation if VREF and VDDA is 3.3V? How can I get the true temperature. E.g. for a chip I have the TS_CAL1 is 4130. What does that mean for 3.3V VREF?

 

BR

Yang

This topic has been closed for replies.
RobK1
RobK1Best answer
Associate II
Apr 8, 2025 7:11 AM UTC

You have to multiply your measurement by (3.3 / 3.0), then do the rest of the calculations.

This is the example ST gives for the 32L0x2:

/* Temperature sensor calibration value address */
 #define TEMP130_CAL_ADDR ((uint16_t*) ((uint32_t) 0x1FF8007E))
 #define TEMP30_CAL_ADDR ((uint16_t*) ((uint32_t) 0x1FF8007A))
 #define VDD_CALIB ((uint16_t) (300))
 #define VDD_APPLI ((uint16_t) (330))
 int32_t ComputeTemperature(uint32_t measure)
 {
 int32_t temperature;
 temperature = ((measure * VDD_APPLI / VDD_CALIB) - (int32_t) *TEMP30_CAL_ADDR );
 temperature = temperature * (int32_t)(130 - 30);
 temperature = temperature / (int32_t)(*TEMP130_CAL_ADDR - *TEMP30_CAL_ADDR);
 temperature = temperature + 30;
 return(temperature);
 }

 

1 reply

RobK1
RobK1Best answer
Associate II
Apr 8, 2025 7:11 AM UTC

You have to multiply your measurement by (3.3 / 3.0), then do the rest of the calculations.

This is the example ST gives for the 32L0x2:

/* Temperature sensor calibration value address */
 #define TEMP130_CAL_ADDR ((uint16_t*) ((uint32_t) 0x1FF8007E))
 #define TEMP30_CAL_ADDR ((uint16_t*) ((uint32_t) 0x1FF8007A))
 #define VDD_CALIB ((uint16_t) (300))
 #define VDD_APPLI ((uint16_t) (330))
 int32_t ComputeTemperature(uint32_t measure)
 {
 int32_t temperature;
 temperature = ((measure * VDD_APPLI / VDD_CALIB) - (int32_t) *TEMP30_CAL_ADDR );
 temperature = temperature * (int32_t)(130 - 30);
 temperature = temperature / (int32_t)(*TEMP130_CAL_ADDR - *TEMP30_CAL_ADDR);
 temperature = temperature + 30;
 return(temperature);
 }