Skip to main content
aralnworb
Associate
May 21, 2019
Question

What is the temperature range of the NUCLEO-L4R5ZI ?

  • May 21, 2019
  • 4 replies
  • 1016 views

Will it operate from 0deg C to 50 deg C?

This topic has been closed for replies.

4 replies

T J
Senior III
May 22, 2019

is that ambient ?

You would expect it to work to 60, but the processor itself should be held down under 75C and so may require heatsink...

the higher temperature alters the propagation delays within the internal bus routing networks.

what frequency are you running, ?

if you lower the frequency and the issue goes away... its a heat issue

did you read out the processor die temperature ?

aralnworb
aralnworbAuthor
Associate
May 22, 2019

​Thanks for your quick response.

Yes, I did mean ambient. We are in the design stages of a project, and just got a late requirement to operate in the 0-50 degC range, and wanted to make sure the nucleo could handle it. According to the STM32-L4R5ZI datasheet the MCU can handle it, but I was concerned about the rest of the nucleo, as there was nothing related to temperature in the Nucleo databrief or user manual that I could find.

T J
Senior III
May 22, 2019

0-50c should be easy,

but you could readout the processor temp ( ambient + 25 roughly depending on clock's configuration, etc.)

and heat it up till it fails...

then you will know the operating temp range with your code running.

the rest of the circuit has been through an oven above 200C, no issue there..

electrolytic caps don't like being hot for a long time. degrading to 50% within a short period.

aralnworb
aralnworbAuthor
Associate
May 22, 2019

​Good suggestion.

And thanks for the feedback, this is very helpful.