Skip to main content
CodeRunner
Associate II
February 28, 2020
Question

What is the proper method to interrupt/signal that new information is ready between core M7 and M4 in an STM32H7 processor?

  • February 28, 2020
  • 1 reply
  • 757 views

I am looking at the STM32H7 reference manual and STM32H745 code examples to determine how to transfer and signal new information between the cores. Currently I see two possibilities: Shared memory and a hardware semaphore/interrupt or shared memory and a software interrupt. If a hardware semaphore is used is it possible to initiate an interrupt from the CM7 core that is received on the CM4 core? I see that the hardware semaphore is primarily used to wakeup a sleeping CM4 core. From the ST provided dual core FreeRTOS example I see that they use a shared message buffer and a software interrupt to signal new information between the cores. Can a hardware semaphore be used to protect shared memory writes and signal new information between cores? Or is the FreeRTOS example the way with a software interrupt the proper way to share/signal information?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
February 28, 2020

HSEM does some of the work, but you still need to manage the memory/cache coherency and write buffers if accessing common memories.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..