Skip to main content
HAbay.1
Associate III
Aug 9, 2021 11:02 PM UTC
Solved

What is the maximum input voltage for the external voltage regulator of the stm32 bluepill?

I am referring to the regulator connected to the usb 5V ( the 5V pin), can it handle a voltage of 12v and step it down to 3.3V for the chip? if not then what is the limit?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 9, 2021 11:56 PM UTC

Check the schematic and placed components on the board you have

RT9193-33 looks to max out at 5.5V

https://www.richtek.com/assets/product_file/RT9193/DS9193-16.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 9, 2021 11:56 PM UTC

Check the schematic and placed components on the board you have

RT9193-33 looks to max out at 5.5V

https://www.richtek.com/assets/product_file/RT9193/DS9193-16.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief
Aug 10, 2021 10:09 AM UTC

Bluepill is produced by many asian companies. Parts used may differ, but assuming 5.5 V max is a good guess.