Skip to main content
Carter Lee
Associate III
Sep 25, 2017 6:52 AM UTC
Solved

What is the fairly common way to implement a flag function?

Posted on September 25, 2017 at 08:52

I'm actually I want to implement some such as a flag function into my code.

But I'm struggling with implementation in c.

What is the fairly common way to implement a flag function?

int trigger =0;

main() {

   while(1) {

   switch (num)

   case0

   case1 : 

trigger = 0

   ..

   case6 : trigger = 1

   

   

   if (trigger==1)

   printf('trigger-on');

   else

   printf('trigger-off');

   

   }

}

As you can see the problem of above is  that if case 6 is activated, then we can see lots of '

trigger-on' printed messages.

But I want this just to do one time with trigger or flag.. 

What is the fairly common way to implement a flag function?

    This topic has been closed for replies.
    ColdWeather
    ColdWeatherBest answer
    Senior
    Sep 25, 2017 7:52 AM UTC
    Posted on September 25, 2017 at 09:52

    First, what has this question with STM micros issues to do? Well, I think there is a lot of ways to solve this. Anyway you have to introduce some variable that would track your prints:

    int last_trigger = -1;   // init to a special value out of 'trigger' range for the very first printout.

    ...

    if (last_trigger != trigger)

    {

          // do print

          last_trigger = trigger;

    }

    3 replies

    After Forever
    Senior III
    Sep 25, 2017 7:34 AM UTC
    Posted on September 25, 2017 at 09:34

    You forgot the breaks for the cases and the functional block for the entire switch.

    Also, after acting on the trigger flag you can turn off the trigger.

    int main() {
     while(1) {
     switch (num) {
     case 0:
     break;
     case 1:
     trigger = 0
     break;
     //..
     case 6:
     trigger = 1
     break;
     default:
     break;
     }
    
     if (trigger == 1) {
     printf('trigger-on');
     trigger = 0;
     } else {
     printf('trigger-off');
     }
     }
    }�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    ColdWeather
    Senior
    Sep 27, 2017 10:37 PM UTC
    Posted on September 27, 2017 at 22:37

    Unfortunately, the code above would print out 'trigger-off' all the time, also at the next pass after a single 'trigger-on' after the case 6. You have either to track the printouts by an additional flag, as I suggested in my reply before, or to reset the 'trigger' to, say, -1 after printing 'trigger-on' out and to add 'if (trigger == 0)' to print 'trigger-off' out.

    OT: what HTML tags to format the source code in the articles?

    ColdWeather
    ColdWeatherBest answer
    Senior
    Sep 25, 2017 7:52 AM UTC
    Posted on September 25, 2017 at 09:52

    First, what has this question with STM micros issues to do? Well, I think there is a lot of ways to solve this. Anyway you have to introduce some variable that would track your prints:

    int last_trigger = -1;   // init to a special value out of 'trigger' range for the very first printout.

    ...

    if (last_trigger != trigger)

    {

          // do print

          last_trigger = trigger;

    }