Skip to main content
Mr_M_from_G
Senior II
December 17, 2021
Solved

What is the difference between pins FDCAN1_TX and FDCAN1_TXFD_MODE ?

Hello ,

in STM32 H742 data sheet I find CAN pind with or without the suffix FD_MODE, but there is no explanation on it. What does that mean? CAN peripheral has only one output for Rx and Tx each. Can't I use those without FD_MODE when using CANFD but only for CAN2.0? How does the pin know which mode is used?

Thank you for some details

Martin

This topic has been closed for replies.
Mr_M_from_G
Mr_M_from_GBest answer
Senior II
December 22, 2021

3 replies

Mr_M_from_G
Senior II
December 20, 2021

Any ideas?

I need this information for a schematics, which pins should I use?

Thanks for any help

Martin

Mr_M_from_G
Mr_M_from_GAuthorBest answer
Senior II
December 22, 2021
mƎALLEm
ST Technical Moderator
February 15, 2022

Dear @Mr_M_from_G​ ,

Indeed, only Rx and Tx are used for FDCAN communication..

All FDCANx_TXFD_MODE & FDCANx_RXFD_MODE occurrences will be removed from datasheets.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.