Skip to main content
Msee
Associate
March 9, 2021
Question

What is the default value for PLLON ? If it is 0, should I put a while(PLLRDY =1)?

  • March 9, 2021
  • 3 replies
  • 884 views

I have an application running on HSE as system clock..and I set the multiplexer to select HSE, totally not using PLL

btw, should I put any configuration to my PLL?

such as PLLON =0, and while(PLLRDY==1) , to “properly configure�? the unused PLL?

Or should I just leave it as what it is by default?

best regards,

mike

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
March 9, 2021

By default it is off, so just leave it as it is.

JW

Tesla DeLorean
Guru
March 9, 2021

You would need for it to be off to reconfigure it. And the processor needs to be clocked from a source that is running.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Msee
MseeAuthor
Associate
March 9, 2021

Hi Tesla,

Thanks for the reply.

It is agreeable to turn PLL off properly, by putting "PLLON =0; while(PLLRDY==1) ", If one wishes to "RE-CONFIGURE" the PLL setting.

But if I don't intend to use PLL at all right from the startup, is "PLLON =0; while(PLLRDY==1)" omittable?

Best Regards,

Mike