Skip to main content
BHall.2
Visitor II
May 12, 2022
Question

What is the code compatibility on the STM32G4xx series?

  • May 12, 2022
  • 2 replies
  • 684 views

If I develop an application for the STM32G431VB for instance, could I drop in a different part in the series with the same footprint and equal or better feature set without retargeting/rebuilding the program? If not, would this work if I stay in the same part type (4x1, 4x3, or 4x4) with larger flash/ram memory? The idea is that given the current disaster of the supply chain, how easy is it to substitute parts in manufacturing?

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 12, 2022

Usually a couple of parts using the same die, check the startup.s examples in the \CMSIS\Device trees as this will show differences in the Interrupt Table, and supported peripheral set.

The CubeMX/IDE tools have a compatible part tool/lister

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
May 13, 2022

Generally, the only guaranteed perfect compatibility with only differences in memory is within models which have the same DS (well, except if they are in different packages or the same package with different pinouts, and that includes the suffixed models - e.g. which have or have not SMPS). The compatibility within a model *number* (or subfamily) is relatively good and remains still quite fair within a family. However, ST likes to throw in surprises here are there (guess how do I know)... so at the end of the day, if you want to avoid nasty surprises, you have to paintstakingly check each planned model for the features you are using.

For some families there are migration notes available.

JW