Skip to main content
Singh.Harjit
Senior
October 11, 2018
Question

What is Radc for STM32H743?

DS12110 Rev 5, notes for Figure 40. says it should be in Table 85 but it isn't. Rain and Cadc are in the Table 85.

​

This topic has been closed for replies.

4 replies

PTowl
Visitor II
November 6, 2018

Hello all,

Would also like to know the answer to this one.

Anyone any idea??

Regards,

CHead
Associate III
April 16, 2019

I suspect it may differ for fast versus slow channels. I would also like to know.

CHead
Associate III
April 17, 2019

I got a reply from ST in a support ticket. Their recommendation is to use table 185 in the datasheet (it’s in the revision V section, but the rep said it applies to revision Y as well).

Singh.Harjit
Senior
April 18, 2019

​The Rev 6 datasheet still calls out Radc in two places and says look for it in two tables. This note should be removed if Radc isn't going to be provided.