Skip to main content
mohsen
Associate
Nov 9, 2016 8:30 PM UTC
Question

What is minimun value of Vref in ADC Nucleo f767?

Posted on November 09, 2016 at 21:30

How much I can put on Vref without lossing bit?

I can read 8 bit without nise (12 bit is noisy) when the Vref is 3.3V. however, my sensor show maximum 12 (decimal). I wan to get more resolution. Therefore I want to change Vref. What is minimum Vref without lossing data or adding noise? can I coonect it to 0.15 V?

#adc
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Nov 9, 2016 9:26 PM UTC
Posted on November 09, 2016 at 22:26

Wouldn't that be in the Data Sheet? Usually such things only allow a small differential between VDD/VDDA

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..