Skip to main content
ABhat.2
Visitor II
Feb 11, 2020 8:14 PM UTC
Question

what happens if more than one version of STMicroelectronics virtual com port driver is intalled on the computer?

I have 1.0, 1.3.1 and 1.4 version of the STM driver installed on my computer. How will it behave?

This topic has been closed for replies.

3 replies

Pavel A.
Feb 12, 2020 12:43 AM UTC

Multiple versions of a driver package can be installed on a Windows machine.

The Device manager will show which driver version is actually active when you connect the device to a PC.

Usually the newest driver package takes precedence, but it depends. TL;DR

-- pa

JoniS
Senior
Feb 12, 2020 4:47 AM UTC

When you attach new device, windows does use the latest driver version by default, but you can force older one from device manager and it should remember it next time for the given device.

Piranha
Principal III
Feb 18, 2020 1:05 PM UTC

Device Manager can also remove the specific currently used version from system by ticking "Delete the driver software for this device.".