Skip to main content
HG?�n
Visitor II
Jun 28, 2019 10:08 AM UTC
Question

What happens, if common mode input voltage for ADC of STM32L431 in differential mode is out of specification?

For example, if there is a larger distortion of 1 V on the input lines (according to datasheet only 0,18 V are allowed), what happens to the ADC and ADC result.

Does this result into a sampling error, and how large would the error be? Or can the ADC even be destroyed?

This topic has been closed for replies.