Question
What are the options for loading program code into the STM32L072RB?
I planned to use the ST-LINK V3SET interface, with the 14 pin target JTAG interface (Table 6 in UM2448 Rev 1), but the JTAG signals/pins/functions are not listed in the datasheets or CubeMX pin configurator.
Does this part not have the JTAG interface? Are the only options for loading code through serial peripherals, for example USB in DFU mode?