Skip to main content
SCort.1
Visitor II
May 30, 2023
Solved

What are the MCUs supported by the X-CUBE-IOD02 and the hardware PHY?

大家好�?我想知�?�X-CUBE-IOD02是�?��?�以移�?到其他MCU?是�?�支�? L6364 以外的 PHY?我该怎么�?�,因为 X-CUBE-IOD02 包�?��?��?库,而�?是所有�?代�?。

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
June 9, 2023

Hello @SCort.1​ and welcome to the Community :) ,

Thanks to develop your posts in English so it helps us, and the users of our community understand your question and try to help you.

I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

Here is the translation of your post using Google translate:

Hello everyone! I wonder if X-CUBE-IOD02 can be ported to other MCU? Are PHYs other than L6364 supported? How can I do this, since X-CUBE-IOD02 contains static libraries, not all source code.

The X-CUBE-IOD02 package is a software expansion for STM32Cube with driver for the L6364 transceiver, a mini-stack library and an IODD configuration file. The package allows you to develop IO-Link sensor applications based on the L6364 mounted on the X-NUCLEO-IOD02A1 expansion board when connected to a NUCLEO-L073RZ or NUCLEO-G071RB development board.

For more explanation, I advise you to refer to UM2749.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thank you

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

1 reply

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
June 9, 2023

Hello @SCort.1​ and welcome to the Community :) ,

Thanks to develop your posts in English so it helps us, and the users of our community understand your question and try to help you.

I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

Here is the translation of your post using Google translate:

Hello everyone! I wonder if X-CUBE-IOD02 can be ported to other MCU? Are PHYs other than L6364 supported? How can I do this, since X-CUBE-IOD02 contains static libraries, not all source code.

The X-CUBE-IOD02 package is a software expansion for STM32Cube with driver for the L6364 transceiver, a mini-stack library and an IODD configuration file. The package allows you to develop IO-Link sensor applications based on the L6364 mounted on the X-NUCLEO-IOD02A1 expansion board when connected to a NUCLEO-L073RZ or NUCLEO-G071RB development board.

For more explanation, I advise you to refer to UM2749.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thank you

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.