Skip to main content
Abin
Associate III
June 11, 2024
Solved

What are the applications of open drain GPIO configuration.

Hai All,

We can configure a GPIO pin either as a Push-Pull or Open-drain configuration. Can anybody explain briefly, what are the applications of Open Drain configuration?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
June 11, 2024

Hello,

For example you can OR many IOs signals just by wiring. No need for an OR gate.

You can also do voltage level shifting from 3.3V IO domain to 5V (since most of STM32 IOs are FT) just by setting the IO to open drain and pull the pin up to 5V via a pull up resistor and you get a 5V output like.

https://www.quora.com/What-is-open-drain-What-are-3-examples-of-application-configuration-about-STM32f

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
June 11, 2024

Hello,

For example you can OR many IOs signals just by wiring. No need for an OR gate.

You can also do voltage level shifting from 3.3V IO domain to 5V (since most of STM32 IOs are FT) just by setting the IO to open drain and pull the pin up to 5V via a pull up resistor and you get a 5V output like.

https://www.quora.com/What-is-open-drain-What-are-3-examples-of-application-configuration-about-STM32f

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.