Skip to main content
Arman Ilmak
Senior
Nov 13, 2021 1:53 PM UTC
Solved

what are all the things I need to create my external loader

Hey guys

Im using stm32h743 and nand flash connected with fmc.

I searched to see how I can create my own external loader for nand(i couldnt find any for nand flash).

I think i just need to adapt Loader_Src.c file to nand flash hal function and a linker to build the .stldr?

Am I on a right way?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Nov 13, 2021 4:52 PM UTC

Step#1 is to build and thoroughly test a BSP from your application space. All the read, write, erase, ECC generation/checking, and correction.

Then map that functionality into the loader and the function entry points that has for these operations.

External Loaders are hard to debug, you're not going to be able to step around with a debugger to solve issues. You can however use whatever board resources you have to output to serial ports, GPIO, LED's, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

3 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Nov 13, 2021 4:52 PM UTC

Step#1 is to build and thoroughly test a BSP from your application space. All the read, write, erase, ECC generation/checking, and correction.

Then map that functionality into the loader and the function entry points that has for these operations.

External Loaders are hard to debug, you're not going to be able to step around with a debugger to solve issues. You can however use whatever board resources you have to output to serial ports, GPIO, LED's, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PFlor.2
Senior II
Feb 13, 2024 8:02 PM UTC

I do know that the following code passes which includes enabling memory mapped mode (see bold).  I also have been using these same quadspi drivers in my application that uses TouchGFX in memory mapped mode as well, so I do know memory mapped mode must be working with TouchGFX, right??  You actually created an external loader for me for this part that I've been using for quite a while but needed to develop my own to support other alternate Flash parts in the future.

uint8_t buffer_test[MEMORY_SECTOR_SIZE];
uint32_t var = 0;

CSP_QUADSPI_Init();

for (var = 0; var < MEMORY_SECTOR_SIZE; var++) {
  buffer_test[var] = (var & 0xff);
}

for (var = 0; var < SECTORS_COUNT; var++) {

    if (CSP_QSPI_EraseSector(var * MEMORY_SECTOR_SIZE,
       (var + 1) * MEMORY_SECTOR_SIZE - 1) != HAL_OK) {

        while (1)
        ; //breakpoint - error detected
    }

    if (CSP_QSPI_WriteMemory(buffer_test, var * MEMORY_SECTOR_SIZE, sizeof(buffer_test)) != HAL_OK) {

        while (1)
        ; //breakpoint - error detected
    }

}

if (CSP_QSPI_EnableMemoryMappedMode() != HAL_OK) {

    while (1)
    ; //breakpoint - error detected
}

for (var = 0; var < SECTORS_COUNT; var++) {
    if (memcmp(buffer_test,
       (uint8_t*) (0x90000000 + var * MEMORY_SECTOR_SIZE),
       MEMORY_SECTOR_SIZE) != HAL_OK) {
        while (1)
       ; //breakpoint - error detected - otherwise QSPI works properly
    }
}

Tesla DeLorean
Guru
Feb 13, 2024 8:12 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..