Skip to main content
keepcoding
Associate III
September 27, 2013
Question

WFI problem: Internal command error

  • September 27, 2013
  • 3 replies
  • 800 views
Posted on September 27, 2013 at 14:10

Hi

I run this very simple code on the STM32F3 Discovery board:

int main(void)
{
__WFI();
return 0;
}

It compiles fine and I can flash it onto the STM without any problems (I'm using the ST-Link). However, when I want to flash the program again, I get the 'Internal Command Error'. This error is independent of the IDE and occurs even with the ST-Link Utility. I then have to select 'connect under reset' option in the ST-Link Utility and then erase the whole chip to get it working again. Any ideas what might cause this problem?
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    September 27, 2013
    Posted on September 27, 2013 at 15:30

    Halting the core precludes the SWD/JTAG executing (operating core) commands it needs too. The debugger can't talk to it. DMA and other lower power operation will also preclude debugger access.

    Also don't return from main(), bad things will happen.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    keepcoding
    Associate III
    September 27, 2013
    Posted on September 27, 2013 at 16:44

    Thanks! So this is normal behaviour. Is there a way to use sleep mode and still be able to flash new code by ST-Link? Do I always need to 'connect under reset' in the future?

    Tesla DeLorean
    Guru
    September 27, 2013
    Posted on September 27, 2013 at 16:53

    Thanks! So this is normal behaviour. Is there a way to use sleep mode and still be able to flash new code by ST-Link? Do I always need to 'connect under reset' in the future?

    Well it's normal that if you turn things off, and clocks/supplies are off, that things cease to function as usual. There are many ways to cause problems, I enumerated some of the most common things. Reseting the core is at least one of the methods that several JTAG/SWD pods use to wrestle control of a system.

    Or you have code to recognize a GPIO/PIN setting, and enter a download safe mode. Or reset with BOOT0 = High

    There might be some DBGMCU controls, or such, that maintain the debug interface in some conditions.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..