Skip to main content
bivin mato
Associate III
Apr 26, 2020 7:07 PM UTC
Solved

WFE examples required for stm32 family?

Hello ,

I would like to get some examples for WFE based sleep . In stm32cube examples, i see that most of them are like WFI based examples. Request someone to help me with this information. Thanks in advance.

Regards,

Vinoth

This topic has been closed for replies.
bivin mato
bivin matoBest answer
Associate III
May 3, 2020 1:39 PM UTC

After searching for while i attempted myself with the understanding from the datasheet.

It works. Hope it helps someone in need. Thanks to @TDK​ .

Code snippet for SEVONPEND = 1 as below

int main(void)
{
	/* Add your application code here */
	__IO uint32_t tmpreg;
 
	/* Enable clock for toggle LED */
	SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
	tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
 
	/* Enable clock for switch input (EXTI) */
	SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
	tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
 
	/* Enable clock for SYSCFG that connects switch to EXTI */
	SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
	tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
 
	/* Configure toggle LED */
	GPIOI->MODER |= GPIO_MODER_MODER15_0;
	GPIOI->PUPDR |= GPIO_PUPDR_PUPDR15_0;
	GPIOI->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15;
	GPIOI->BSRR= GPIO_BSRR_BS15; // Reset
 
	/* Configure switch input */
	GPIOC->PUPDR = 0;
	GPIOC->MODER = 0;
	SYSCFG->EXTICR[3] = 0x20;
	EXTI->IMR = 0x2000;
	EXTI->EMR = 0;
	EXTI->RTSR = 0x2000;
 
	SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SEVONPEND_Msk));
 
	/* Infinite loop */
	while (1)
	{
		/* Set SLEEPDEEP bit of Cortex System Control Register */
		SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
 
		/* Ensure that all instructions done before entering SLEEP mode */
		__DSB();
		__ISB();
 
	 /* Request Wait For Event */
	 __SEV();
	 __WFE();
	 __WFE();
 
		/* Reset SLEEPDEEP bit of Cortex System Control Register */
		SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP_Msk);
 
	 /* Clear the flag responding to the event */
	 EXTI->PR = 0x2000;
		while (EXTI->PR != 0);
 
		/* Clear the pending flag responding to the event in NVIC */
		NVIC_ClearPendingIRQ(EXTI15_10_IRQn);
 
		ToggleLed();
	}
 
}

Code snippet for SEVONPEND = 0 as below

int main(void)
{
	/* Add your application code here */
	__IO uint32_t tmpreg;
 
	/* Enable clock for toggle LED */
	SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
	tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
 
	/* Enable clock for switch input (EXTI) */
	SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
	tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
 
	/* Enable clock for SYSCFG that connects switch to EXTI */
	SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
	tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
 
	/* Configure toggle LED */
	GPIOI->MODER |= GPIO_MODER_MODER15_0;
	GPIOI->PUPDR |= GPIO_PUPDR_PUPDR15_0;
	GPIOI->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15;
	GPIOI->BSRR= GPIO_BSRR_BS15; // Reset
 
	/* Configure switch input */
	GPIOC->PUPDR = 0;
	GPIOC->MODER = 0;
	SYSCFG->EXTICR[3] = 0x20;
	EXTI->IMR = 0;
	EXTI->EMR = 0x2000;
	EXTI->RTSR = 0x2000;
 
	/* Infinite loop */
	while (1)
	{
		/* Set SLEEPDEEP bit of Cortex System Control Register */
		SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
 
		/* Ensure that all instructions done before entering SLEEP mode */
		__DSB();
		__ISB();
 
	 /* Request Wait For Event */
	 __SEV();
	 __WFE();
	 __WFE();
 
	 /* Reset SLEEPDEEP bit of Cortex System Control Register */
		SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP_Msk);
 
		ToggleLed();
	}
 
}

2 replies

TDK
Apr 26, 2020 7:53 PM UTC

> WFE examples required for stm32 family?

Might want to narrow down STM32 family a bit. There are a lot of products out there.

Doesn't seem to be many CubeMX examples that use WFE. But here is one:

https://github.com/STMicroelectronics/STM32CubeH7/blob/e261d820b398846a94f22f4aeb32d86c29546efb/Projects/STM32H747I-EVAL/Applications/OpenAMP/OpenAMP_PingPong/CM4/Src/main_cm4.c

When I want examples, sometimes I use the raw GitHub search to find where things are used. A lot of hits are from the definition file, but some are in project usage:

https://github.com/search?q=PWR_SLEEPENTRY_WFE+filename%3A*.c+language%3AC+language%3AC&type=Code

"If you feel a post has answered your question, please click ""Accept as Solution""."
bivin mato
bivin matoAuthorBest answer
Associate III
May 3, 2020 1:39 PM UTC

After searching for while i attempted myself with the understanding from the datasheet.

It works. Hope it helps someone in need. Thanks to @TDK​ .

Code snippet for SEVONPEND = 1 as below

int main(void)
{
	/* Add your application code here */
	__IO uint32_t tmpreg;
 
	/* Enable clock for toggle LED */
	SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
	tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
 
	/* Enable clock for switch input (EXTI) */
	SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
	tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
 
	/* Enable clock for SYSCFG that connects switch to EXTI */
	SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
	tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
 
	/* Configure toggle LED */
	GPIOI->MODER |= GPIO_MODER_MODER15_0;
	GPIOI->PUPDR |= GPIO_PUPDR_PUPDR15_0;
	GPIOI->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15;
	GPIOI->BSRR= GPIO_BSRR_BS15; // Reset
 
	/* Configure switch input */
	GPIOC->PUPDR = 0;
	GPIOC->MODER = 0;
	SYSCFG->EXTICR[3] = 0x20;
	EXTI->IMR = 0x2000;
	EXTI->EMR = 0;
	EXTI->RTSR = 0x2000;
 
	SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SEVONPEND_Msk));
 
	/* Infinite loop */
	while (1)
	{
		/* Set SLEEPDEEP bit of Cortex System Control Register */
		SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
 
		/* Ensure that all instructions done before entering SLEEP mode */
		__DSB();
		__ISB();
 
	 /* Request Wait For Event */
	 __SEV();
	 __WFE();
	 __WFE();
 
		/* Reset SLEEPDEEP bit of Cortex System Control Register */
		SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP_Msk);
 
	 /* Clear the flag responding to the event */
	 EXTI->PR = 0x2000;
		while (EXTI->PR != 0);
 
		/* Clear the pending flag responding to the event in NVIC */
		NVIC_ClearPendingIRQ(EXTI15_10_IRQn);
 
		ToggleLed();
	}
 
}

Code snippet for SEVONPEND = 0 as below

int main(void)
{
	/* Add your application code here */
	__IO uint32_t tmpreg;
 
	/* Enable clock for toggle LED */
	SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
	tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
 
	/* Enable clock for switch input (EXTI) */
	SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
	tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
 
	/* Enable clock for SYSCFG that connects switch to EXTI */
	SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
	tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
 
	/* Configure toggle LED */
	GPIOI->MODER |= GPIO_MODER_MODER15_0;
	GPIOI->PUPDR |= GPIO_PUPDR_PUPDR15_0;
	GPIOI->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15;
	GPIOI->BSRR= GPIO_BSRR_BS15; // Reset
 
	/* Configure switch input */
	GPIOC->PUPDR = 0;
	GPIOC->MODER = 0;
	SYSCFG->EXTICR[3] = 0x20;
	EXTI->IMR = 0;
	EXTI->EMR = 0x2000;
	EXTI->RTSR = 0x2000;
 
	/* Infinite loop */
	while (1)
	{
		/* Set SLEEPDEEP bit of Cortex System Control Register */
		SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
 
		/* Ensure that all instructions done before entering SLEEP mode */
		__DSB();
		__ISB();
 
	 /* Request Wait For Event */
	 __SEV();
	 __WFE();
	 __WFE();
 
	 /* Reset SLEEPDEEP bit of Cortex System Control Register */
		SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP_Msk);
 
		ToggleLed();
	}
 
}