Skip to main content
ambrose
Associate II
July 7, 2015
Question

Weird/Not fully understood behaviour of HRTIM

  • July 7, 2015
  • 2 replies
  • 938 views
Posted on July 07, 2015 at 13:26

Iam having big problems with the high resolution timer on the STM32f334microcontroller.

I am using a period of 0xD3C2, this would normally mean that writting 0xD3C2 to a compare register is full duty cycle (or zero  - actually 0x60, as I am running at 4GHz - depending on the polarity). - 

(I use compare registers one and two for two separate circuits).

And that the duty cycle will reduce progressively as you reduce the number. But this is not the case. what I have observed is that

0xD3C2 to a compare register is full duty cycle, but the behaviour of the hardware is unpredictable between a value of 0xD3C2 and 0xD3A2(ish).

Also, it seems that the act of writing to the compare register creates unusual spikes in the controlled circuits. I do know that the reference manual

specifies minimum and maximum values for compare registers depending on the CKPSC[2:0] values. I guess that these values are not

necessarily fixed, but depends on the actual period of PWM.

I am not sure exactly why it behaves odd, but could any one please enlighten me on this.

(I am running the PWM at about 85kHz)

Thanks.

#stm32f334 #hrtim
This topic has been closed for replies.

2 replies

Amel NASRI
ST Technical Moderator
July 9, 2015
Posted on July 09, 2015 at 12:04

Hi,

Did you have a look to the HRTIM CookBook (

http://www.st.com/web/en/resource/technical/document/application_note/DM00121475.pdf

)? It explains how to do in order to program the HRTIM and provides some samples for typical use cases.

-Mayla-

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
ambrose
ambroseAuthor
Associate II
July 21, 2015
Posted on July 21, 2015 at 10:58

Thanks for the response. Yes I have. I find that simply avoiding 100% duty cycle will make it behave normally, I just wanted to know if anyone has similar experience and know a better way. The reference manual does not say anything about this.