Skip to main content
Masanori Toyoda
Associate
Feb 21, 2017 7:42 AM UTC
Question

We need a large sum of STM32W108CBU64TR.

Posted on February 21, 2017 at 08:42

Hi, members.

I'm a chief engineer in charge of developping information display with touch faunction.

And my team are developping fat stylus pen that can communicate with touch panel.

Actually though under mas production, STM chips are short for further plan.

If you know who has a plenty of stock of them, please tell me immediately. 

I appreciate your help.

    This topic has been closed for replies.

    17 replies

    T J
    Senior III
    Feb 21, 2017 1:41 PM UTC
    Posted on February 21, 2017 at 14:41

    that part is marked as obsolete !

    luckily for you,

    many of these chips are interchangeable,

    although the code may have to be tweaked.

    Masanori Toyoda
    Associate
    Feb 22, 2017 1:27 AM UTC
    Posted on February 22, 2017 at 01:27

    Dear Mr.Nick,

    Thank you for your advice.

    I have a question.

    What do you mean that many of these chips are interchangeable?

    Actually, I have thought that STM32W108CBU61, STM32W108CBU62, STM32W108CBU63 can be

    substituted for STM32W108CBU64.

    But I have heard it was wrong.

    I would like you to tell me what you told in detail.

    I appreciate your help and cooperation.

    Regard,

    Masanori Toyoda

    T J
    Senior III
    Feb 22, 2017 1:40 AM UTC
    Posted on February 22, 2017 at 01:40

    on page 279 of the data sheet;

    the 61 Vs 63 Vs 64 reference:

    '

       This P/N is under specific ordering conditions. Please refer to your nearest ST sales office.

       1 = Ember ZigBee stack, available on 128 Kbyte devices only.

       3 = RF4CE stack

       4 = IEEE 802.15.4 media access control

    '

    generally, the ST processors have the same pin outs, PA4, PA5 PB7 for example are generally always in the same position.

    However, in this case, the IEEE 802.15.4 media access control is unique to the STM32W108CBU64TR.

    You can ask on this forum if there is another processor that has this the IEEE 802.15.4 media access control.

    then you must check the pin outs are the same, usually yes.

    then you must adjust your firmware to accommodate the slight variations in processors.

    ie, the internal clock may be higher, so timers/timeout values may have to be adjusted.  etc.

    Tesla DeLorean
    Guru
    Feb 21, 2017 9:23 PM UTC
    Posted on February 21, 2017 at 22:23

    These parts were discontinued close to 4-5 years ago (SiLabs bought Ember, one of the primary stack vendors). They are specialize WiFi parts (STM32W) and really don't have much relationship to other STM32F1xx parts.

    ST Sales might have some idea if any distributor holds any volume at this point.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Masanori Toyoda
    Associate
    Feb 22, 2017 1:40 AM UTC
    Posted on February 22, 2017 at 01:40

    Dear Clive,

    Thank you for your information and advice.

    Actually we had the last order of STM32W108CBU64 for ST-micro in 2015.

    Unfortunately, there was a gap between the initial prospect and the actual demand.

    If you know, I would like you to tell me how to do to ask to ST sales for this matter.

    I appreciate your help and cooperation.

    Regards,

    Masanori Toyoda

    richard239955_stm1
    Associate III
    Feb 23, 2017 6:38 PM UTC
    Posted on February 23, 2017 at 19:38

    I just read through this conversation.

    Have you been in direct contact with your STMicroelectronics representative? The FAE's in our area are great at helping to solve problems.

    Instead of spinning a new board to accommodate a different chip with a different pinout, why not use a carrier. Mount the replace chip on a daughter card/carrier and then mount that assembly on you current board. This could buy you time to develop a new board a go through the full development, prototype, debug, manufacturing cycle.

    Just thinking out loud.

    Masanori Toyoda
    Associate
    Feb 27, 2017 12:38 AM UTC
    Posted on February 27, 2017 at 00:38

    Dear Richard-san,

    Thank you for your advice.

    Actually we have already mas-produced this product with this chip.

    Then we can't add anything for current model withiout new Authentication.

    We could not contact ST diectly because our local agent would not forgive us it.

    Actually they are helping us instead of ST. Unfortunately the valid result is none for us.

    I appreciate yor help and coopeation.

    Best Regards,

    Masanori Toyoda

    richard239955_stm1
    Associate III
    Feb 27, 2017 8:09 AM UTC
    Posted on February 27, 2017 at 08:09

    Did your local agent not tell you way back when that the component

    you're so desperately looking for was obsolete?

    If they failed to tell you, then they should be paying for the costs to

    re-design the product with a supported and current product.

    I wish you all the best.

    Laurent VERA
    ST Employee
    Feb 26, 2017 8:19 PM UTC
    Posted on February 26, 2017 at 21:19

    Dear Toyoda San,

    Unfortunately this product was terminated. ST is not in a position to manufacture this product anymore. There might be stock at local distributors, but no product left in ST warehouse. 

    If you are located in Japan, I recommend that you contact our sales office in Tokyo or Osaka to check whether they can help. Contact details are on st.com

    Masanori Toyoda
    Associate
    Feb 27, 2017 12:25 AM UTC
    Posted on February 27, 2017 at 00:25

     ,

     ,

    Dear Vera-san,

    Thank you for your advice.

    Actually we have serched whether there are stock of the device in Japan, US, and china so on.

    I could get about five hundred pieces only.

    Thanks.

    Masanori Toyoda

    STMicroelectronics Community <,https://community.st.com/?et=watches.email.thread>,

    Re: We need a large sum of STM32W108CBU64TR.

    reply from Laurent VERA<,https://community.st.com/0D70X000006SPVVSA4