Question
We can add DMA interrupt for the stm32f042x6 ?
We have 3 DMA interrupts DMA1_Channel1_IRQHandler,
DMA1_Channel2_3_IRQHandler,
DMA1_Channel4_5_6_7_IRQHandler, i need use 3 interrupts beer 2 channels because i use 3 usart with DMA (3 x channels for TX and channels for RX).
1- i can split the channels 4_5_6_7 to two interrupts DMA1_Channel4_5_IRQHan & DMA1_Channel6_7_IRQHan ?
2- i can add channel to interrupt DMA1_Channel1_IRQHandler ?
thanks for the help