Skip to main content
MHase
Associate III
September 22, 2020
Question

We are using the STM32F746 in combination with an exernal SD-RAM. The clock rate for the RAM is set to a frequency of 96 MHz.

  • September 22, 2020
  • 1 reply
  • 655 views

We are using the STM32F746 in combination with an exernal SD-RAM.

The clock rate for the RAM is set to a frequency of 96 MHz.

At radiated emission measurement we are above the limit line at 192MHz (double RAM clock)

Is there a possibility to activate jittering or any other option to reduce the radiated emmisions of the electronic system?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
September 22, 2020
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..